HomeServer/FacilityServer redundant operation
These instructions describe set-up and operation of two HomeServers (HS) or FacilityServers (FS) in redundant operation.
These instructions describe set-up and operation of two HomeServers (HS) or FacilityServers (FS) in redundant operation.
The function template is used in conjunction with the Schüco KNX gateway and the Gira HomeServer "Window/slider element" logic node from the "Schüco\Element type" folder, in order…
The module is used to control redundant operation of two HomeServers (HS) or FacilityServers (FS). Function: In connection with a Gira KNX switching actuator, the active HomeServer…
The function template is used for the status display and control of redundant operation of two Gira HomeServers (HS)/FacilityServers (FS). The function template enables the…
This module enables you to control and query your Smart Home via the HomeServer by voice.
The customer owns a DCS-IP-gateway and a HomeServer and would like to be able to save the image of the door communication camera in the image archive of the HomeServer. The image…
Modern home and building automation systems often use various other systems and technologies. In the latest version, the NETx BMS Server also offers an interface to Gira…
The signalling system allows the existing sensors of a KNX installation to be connected to the Gira HomeServer to monitor a building or building part. The signalling system in the…
The signalling system allows the existing sensors of a KNX installation to be connected to the Gira HomeServer to monitor a building or building part. The signalling system in the…
With the HomeServer Projectmanager you can easily organize and share your HomeServer and FacilityServer projects from Gira and Feller. A simple check-in/check-out function gives…
The global library enables retrieval of Gira device portal weather forecast data using the Gira HomeServer or FacilityServer (HS or FS) and to process this data at communication…
The module evaluates a 3-byte telegram according to DPT 232.600 (colour RGB). The HomeServer makes the current values for the RGB colours as 1-byte available at the outputs. The…
The global library enables the visualisation and operation of a signalling system realised in the HomeServer via an AjaxVisu. The visualisation is optimised for display within a…
The bar graph plug-in is used to display HomeServer archive data in the form of a bar graph. Graphs with only one data archive (single graph) or graphs with 2 data archives (double…
Evaluation of a code in the HomeServer and testing of time zones.
The function template calls up a scene saved in the HomeServer.
Sample project for controlling the DCS Communicator via UDP telegrams from the visualisation of the HomeServer.
Sample project for controlling the HSPlugInClient via IP telegrams from the visualisation of the HomeServer.
The signalling system plug-in is used in connection with the logic modules for realising a signalling system with the Gira HomeServer to display the current system states of the…
The function template is used for creating individual RGB(W) lighting moods that are set, stored or called up using HomeServer lighting scenarios.
Easily activate the automatic door opener on your door communication system to grant guests or customers automatic access.
The function template displays the garbage status and offers the option of resetting it.
Realises automatic watering of the garden depending on a weather station with rain sensor, the cistern fill level and the forecast chance of rain without additional sensors.
The module illustrates the function of a timer with a freely selectable time. By using several modules, complex sequences can be set up with an editable sequence.
The global library contains the output of positive or negative acknowledgements at a door station of the Gira door communication system, controlled by a logic module in the Gira…
The module uses an ongoing meter reading to calculate the current daily value, the daily value of the previous day, the meter reading of the previous day, the average of the value…
Specification of a one-time code and evaluation of the code entered on the keypad in the HomeServer.
The function template is used to display lists which are available in text form. Application examples: • Display of a list of fault messages (realised with logic modules from…
The logic node is used in conjunction with the KNX gateway from the company Schüco in order to evaluate the latest status or event information from the Schüco system. Hint: The…
The function template is used to visualise the status of heating, air conditioning or ventilation systems. Information with 2 states (1-bit) for third-party systems can be…
The function template is used to visualise the status of heating, air conditioning or ventilation systems. Information on temperature (e.g. flow or return temperature of a heating…
The module adds the values of the up to 10 inputs and makes the result available at the output.
The sample project contains a complete template for realising a query function in the QuadClient with the functions of the main menu icons and function templates from Expert…
The module converts positive integers into the corresponding other number system. In this way, decimal values (max. 32-bit) can be converted into the binary system and output as a…
The logic module calculates cyclically repeating collection dates and provides information about upcoming collection of a garbage type (e.g. bio-waste, green bin). One module…
The sample project contains a query function for 15 group addresses which can be switched on/off via the building structure of the QuadClient. The states are visualised within the…
The module is for calculation of the dewpoint depending upon relative humidity in % and air temperature.
The module is for calculation of the frost point depending upon relative humidity in % and air temperature.
Import file for 25 new QuadClient menu symbols .
The logic module keeps the desired brightness in a room constant based on the measured brightness value.
Multi-line display and retentive ring memory of values.
The module determines the date of the current day as well as the past 7 days and outputs the date as a 14-byte text in the form dd.mm.yyyy for each day.
The module cyclically calculates the difference between a target date and the current date. The number of days until the target date is reached is sent out at the outputs. In…
The logic module is used in connection with Gira actuators which support current measurement. Using the current values sent via the bus, the module calculates the current power…
The logic module KNX status (forced) operating mode (1-byte, DPT 20.102) evaluates the 1-byte object "KNX status operating mode" or the object "KNX status forced operating mode" of…
The module is used in connection with the Gira room temperature controllers to evaluate the object "Controller status" in the configuration status controller = controller in…
The module is used in connection with the Gira room temperature controllers to evaluate the object "Controller status" in the configuration status controller = controller in…
The module evaluates group feedback according to DPT 27.001.
The module is used to determine the number of active inputs (e.g. open windows) of up to 10 inputs.
The function template displays a fault for selectable states
The function template displays the status of a window (open or tilted). It enables operating the window via KNX when electric motor drives are also used.
The function template shows the status for a selectable variable as a light signal or a smiley.
The function template is used to display the status. Either a symbol or a text is used to display the status.
The module checks whether the value lies inside or outside a range. The range is defined by an upper and lower limit. If the comparison value is on or below the lower limit, a 1 is…
This module switches the selected input to the output. The output is then given the value of the selected input. This module could bes used to switch a system between the modes…
The module evaluates the switching status of RGB(W) lights where feedback is separate for each colour component through a 1-byte object and no feedback object is available for the…
Display of the 14-byte texts of the EIB alarm control unit
The function template enables scenes to be called up and taught up via the auxiliary function.
The module determines the date of the current day as well as the upcoming 7 days and outputs the date as a 14-byte text in the form dd.mm.yyyy for each day.
The sample project shows a measured value for the current day and the past 7 days in the form of a bar graph within the MiniVisu.
The global library contains all available IP commands for controlling the HSPluginClient (e.g. on a Gira Control).
The function template is used to operate and display the status of fan coil controllers. The number of fan speeds can be selected via the behaviour.
The function template is used to operate and display the status of fan controllers. The number of fan speeds can be selected via the behaviour. The following behaviours are…
The module outputs a 3-byte telegram according to DPT 232.600 (colour RGB). Values in the format 0-255 or in percent can be set for each of the three colours.
A 3-byte value is converted to 24 bits and output via 24 outputs.
The module is used to control fan coils in conjunction with fans in the heating and cooling operating modes in the Automatic or Manual mode. The control of the display elements and…
The module is used to control a 3-speed fan. The basic operation of the fan was modelled on the operation of car air conditioners. Manual mode: Following release, the user can…
The module is used to control a 5-speed fan. The basic operation of the fan was modelled on the operation of car air conditioners. Manual mode: Following release, the user can…
The logic module is used to specify a setpoint value depending on a (KNX room temperature controller) operating mode. The module has been realised to enable operation via the…
The KNX alarm control unit plug-in is used in connection with the Gira alarm control unit KNX (Order Number 1142 00) to display the current system states of the alarm control unit…
The Resources plug-in is used to visualise current measured values and display balances or progressions. The following energy types can be visualised with the plug-in. 1…
This function template is used for status display of Gira smoke alarm devices with an in-built KNX module. The function template enables the following selection options: Smoke or…
The function template is used to represent individual displays/operations for up to 4 1-bit communication objects from the audio range. The number of fields (1-4) and the symbols…
The function template is used to change over the source and set the volume of audio sources. The number of sources and the use of the mute function are determined using parameters…
The function template is used to represent individual displays/operations for up to 4 1‑bit communication objects. The number of fields (1-4) and the symbols to be displayed are…
The function template is used to display an individual user, room or audio source selection for up to four objects. The number of fields (one to four) and the symbols to be…
The sample project for the ETS 4 shows the parameterisation of the KNX presence detector Comfort (Gira Art. No. 2106 xx) as an individual device in the function ceiling observer…
HSConnect FritzDect ist ein Logikbaustein für den Gira HomeServer. Mit diesem Baustein kann eine an die FRITZ!Box angebundene DECT-Steckdose “FRITZ!DECT 200” gesteuert…
E-Mobilität wird ein immer wichtigeres Thema. Nun wurde die Möglichkeit geschaffen, E-Autos und deren Ladung intelligent mit dem Gebäude zu vernetzen. Somit erreicht man eine…
ScenarioPro eröffnet dem Integrator in Sachen Szenen völlig neue Möglichkeiten. Da sich Szenen jederzeit inkl. der zugerhörigen Objekte gebäudeweit anlegen und ändern lassen, muss…
Mit HSConnect SONOS lassen sich Sonos-Player nahtlos in bestehende Visualisierungen und KNX-Installationen integrieren. Steuern Sie ab sofort Ihre Sonos-Player bequem und…
SolarLog ist ein durchdachtes System zum Management und zum Monitoring der eigenen Photovoltaik-Anlage. Alle kompatiblen Wechselrichter werden unterstützt und können in die…
SolarLog ist ein durchdachtes System zum Management und zum Monitoring der eigenen Photovoltaik-Anlage. Alle kompatiblen Wechselrichter werden unterstützt und können in die…
Der Kostal Batteriewechselrichter sorgt für eine direkte Ladung des Batteriespeichers von der Zuleitung aus der PV Anlage. Dabei managt er unter Berücksichtigung des Ladestands…
Machen Sie Ihren QC-Client noch persönlicher und individueller. Durch die Funktionsvorlage Text, kannst Du Hinweise, Kontaktdaten oder sonstige Textinformationen darstellen. Per 14…
Egal ob anzeigen oder bedienen. Mit dieser Funktionsvorlage können Sie völlig frei Werte darstellen und verändern. Inkl. Überschrift, Einheit und Kommastellen. So ist die Bedienung…
Zeigen Sie bis zu 20 Zustände im Ampel Prinzip in nur einer Zeile an und verwalten Sie die Störungen durch Quittung und Reset. Durch das Ampelsystem als Sammelmeldung sehen Sie…
Bedienen Sie Ihren Fernseher, Musikanlage, Receiver oder ähnliches komfortabel und direkt im Quad Client. Alle wichtigen Funktionen die Sie benötigen sind enthalten, wie Programm…
Nutzen Sie das PopUp um zahlreiche Funktionen wie Szenen, Einstellungen, Lüftung, Musik und vieles mehr praktisch und übersichtlich in einer QC Zeile zu integrieren. Sie können die…
Farblichter aller Art und natürlich Weißlicht mit Temperaturvorgabe, können Sie flexibel von allen Endgeräten bedienen und anzeigen. Passen Sie die Slider an Ihre Bedürfnisse an…
Einen Sleep-Timer und WakeUp-Timer haben Sie nun direkt in der Oberfläche und können elegant eine Schaltzeit anlegen, die auch nur einmal ausgeführt wird. Natürlich eignet es sich…
Hier findest Du kleine und auch etwas größere Helfer, die den Umgang und Aufbau einer Logik wesentlich vereinfachen. Einige Logikbausteine werden sicherlich bald Deine besten…
Mach Dein Gebäude sicherer und nütze vorhandene Melder um es zu Schützen. Verwalte welcher Melder aktiv sind oder was bei diversen Alarmen passieren soll. Kriege sofort eine…
Wenn einmal etwas nicht in Ordnung ist musst Du es auch wissen. Verwalte und Überwache Deine Störmeldungen einfach und übersichtlich. Durch die Statusanzeigen und Quittung/Reset…
Kennst Du Deinen Energieverbrauch? Weißt Du wie viel Energie Du in der Stunde oder am Tag verbrauchst? Mit dem Energiezähler kannst Du Deinen Verbrauch erfassen, diesen in…
Lass Deine Jalousie oder Rollladen nach Sonnenstand völlig automatisch Dein Gebäude beschatten, damit es Dich nicht blendet oder es zu warm wird. Aber nur, wenn die Sonne auch…
Lass Deine Bewegungsmelder intelligent werden. Schalte und Dimme unterschiedliche Lichter zu unterschiedlichen Zeiten mit unterschiedlicher Verzögerung. Sei frei und vergebe die…
Deine Beleuchtung im Raum passt sich automatisch der benötigten Helligkeit an. Nütze einen Helligkeitsfühler (Innen oder Außen) um Deine Beleuchtungsstärke zu regeln. So hast Du…
Binde Deine Lüftung in Dein Gebäude ein und lass diese automatisiert oder manuell laufen. Nütze Temperatur, Feuchtigkeit und CO2 Werte um zu automatisieren. Lege einzelne Stufen…
Neben der direkten Ansteuerung der hue-Leuchten (Schalten, Dimmen, Farbwahl) bietet der Controller einen internen Szenenspeicher für bis zu 64 Szenen. Die Szenen lassen sich…
Mit QC-Camera können Videostreams von IP-Kameras im Gira QuadClient dargestellt werden. QC-Camera unterstützt alle gängigen Videoformate, Codecs und Auflösungen inklusive des…
Dieses Template steuert Klimaanlagen (Sanyo und Panasonic), die Betriebsartenumschaltung, Lüfterstufen und/oder Lüftstromrichtungen zur Steuerung anbieten.
Dieses Template visualisiert Meldegruppen-Zustände und steuert, ob diese intern oder extern gesperrt oder entsperrt werden sollen. Außerdem zeigt das Template an, ob es sich um…
Dieses Template visualisiert die wichtigsten Funktionen eines Sonos Zone-Players. (Wiedergabe/Stopp, Nächster/Vorheriger Titel, Lautstärke)
Die Belegung von Gebäuden oder Räumen erfolgt über den bekannten Microsoft Outlook-Terminkalender. Die hier hinterlegten Zeitprofile steuern Licht, Heizung und Lüftungsanlagen…
Dieses Template visualisiert die Einstellungen für eine Sonnenschutzsteuerung (Automatik an/aus, Preset für Position und Lamellenstellung).
Mit dem SCRIPTING Logic Node lassen sich Berechnungen, Textverarbeitung und individuelle Logik in einem einzigen Block bündeln. Dadurch ersetzen Sie mehrere Formel-, Formatierungs-…
Steuerung und Integration kompatibler sonoro Musiksysteme in Gira Smart-Home-Umgebungen. Die Anwendung ermöglicht die zentrale Bedienung wichtiger Audiofunktionen direkt über den…
Die Anleitung beschreibt die Parametereinstellungen am Tastsensor 3 plus , um eine optimale Anbindung an folgende Funktionsvorlagen des Quadconfig aus dem Ordner Heizung / Klima /…
Stetig steigender Kostendruck, angespannte Haushaltslagen, Personalengpässe oder der sorgsamere Umgang mit Energieressourcen und der Umwelt sind Herausforderungen, denen sich immer…
Steuern Sie einen vollständigen Konferenzraum und die darin enthaltenen technischen Geräte ganz leicht über eine zentrale Visualisierung.
Der Logikbaustein wird zur Einzelraum-Temperaturregelung verwendet. In Abhängigkeit der Betriebsart, des aktuellen Temperatur-Sollwerts und der Raumtemperatur kann für einen…
Der Logikbaustein wird zur Einzelraum-Temperaturregelung verwendet. In Abhängigkeit der Betriebsart, des aktuellen Temperatur-Sollwerts und der Raumtemperatur kann für einen…
Attention! Only for Gira HomeServer 4 or Gira FacilityServer 4.
Software for the Gira HomeServer 4 or Gira FacilityServer 4.
Connection to the Gira HomeServer/FacilityServer for Apple products. Version 10.7, April 2012, size 2.31 kB. Important: limited compatibility to ETS4! Please use these products in…
Project file for updating the USB data interface, from ETS5.
Mit dieser Datei können Sie die Firmware vom Gira HomeServer/FacilityServer auf die Version 4.6.0 via USB-Stick downgraden. Die Datei kann ab den folgenden Indexständen verwendet…
Anwendungsbeispiel Türöffnerautomatik automatisch aktivieren
Anwendungsbeispiel JPEG-Abruf
HomeServer Logikmodul "Türöffnerautomatik einschalten / ausschalten / abfragen".
HomeServer Logikmodul "Status Türöffnerautomatik auswerten".
HomeServer Logikmodul "Status JPEG-Abruf auswerten".
HomeServer Logikmodul "Sprachansage senden".
HomeServer Logikmodul "Status Ansage auswerten"
HomeServer Logikmodul "Weiterleitung senden".
HomeServer Logikmodul "Status Weiterleitung auswerten".
Additional information
Documentation for software development of HomeServer logic, plugins, templates and URL Endpoint.
The DCS Communicator PlugIn Client in the Quad Client calls up the file „TKS-Communicator.exe“ via a parameter transfer. The events are controlled via UDP telegrams.
This document describes the setup of Amazon Alexa in connection with the Gira S1 and the Gira X1 or Gira HomeServer.
This document describes the setup of Google Assistant in connection with the Gira S1 and the Gira X1 or Gira HomeServer.
Operating instructions.
This document describes how to start up a Gira G1 (2nd generation) and set the parameters for the various applications.
Gebrauchsanleitung.
Controllo centralizzato della domotica: da casa e da remoto.
Controllo centralizzato della domotica: da casa e da remoto.
Zur Steuerung des Smart Home via HomeServer für Villen & mehr.
GNU General Public License.
EC Declaration of conformity
PSTI Statement of Compliance
Funktionaler Angebotstext zum Gira HomeServer/FacilityServer. Format Excel. Version 1.3.1 Stand Februar 2016.
Das vorliegende Musterprojekt soll dem Inbetriebnehmer / Projektanten als Beispiel dienen, wie sich eine individuelle Visualisierung auf Basis der ab Experte 4.7.0 verfügbaren…