Downloads & Software-Updates

Suche nach homeserver

AppShop Software (113)

HS/FS redundant operation

The module is used to control redundant operation of two HomeServers (HS) or FacilityServers (FS). Function: In connection with a Gira KNX switching actuator, the active HomeServer…

Artikel-Nr. 7890105

Version 1.2

HS/FS redundant operation

The function template is used for the status display and control of redundant operation of two Gira HomeServers (HS)/FacilityServers (FS). The function template enables the…

Artikel-Nr. 7890104

Version 1.0

Day of the week display

The global library enables retrieval of Gira device portal weather forecast data using the Gira HomeServer or FacilityServer (HS or FS) and to process this data at communication…

Artikel-Nr. 7890035

Version 1.0

Signalling system visualisation

The global library enables the visualisation and operation of a signalling system realised in the HomeServer via an AjaxVisu. The visualisation is optimised for display within a…

Artikel-Nr. 7890054

Version 1.0

Bar graph

The bar graph plug-in is used to display HomeServer archive data in the form of a bar graph. Graphs with only one data archive (single graph) or graphs with 2 data archives (double…

Artikel-Nr. 7890091

Version 1.1

Signalling system

The signalling system plug-in is used in connection with the logic modules for realising a signalling system with the Gira HomeServer to display the current system states of the…

Artikel-Nr. 7890093

Version 1.2

RGB(W) Scenes

The function template is used for creating individual RGB(W) lighting moods that are set, stored or called up using HomeServer lighting scenarios.

Artikel-Nr. 7890113

Version 1.0

Timer

The module illustrates the function of a timer with a freely selectable time. By using several modules, complex sequences can be set up with an editable sequence.

Artikel-Nr. 7890046

Version 1.0

Daily meter value

The module uses an ongoing meter reading to calculate the current daily value, the daily value of the previous day, the meter reading of the previous day, the average of the value…

Artikel-Nr. 7890058

Version 1.0

List display

The function template is used to display lists which are available in text form. Application examples: • Display of a list of fault messages (realised with logic modules from…

Artikel-Nr. 7890090

Version 2.0

Converter: Decimal - Binary

The module converts positive integers into the corresponding other number system. In this way, decimal values (max. 32-bit) can be converted into the binary system and output as a…

Artikel-Nr. 7890072

Version 1.0

Garbage notification

The logic module calculates cyclically repeating collection dates and provides information about upcoming collection of a garbage type (e.g. bio-waste, green bin). One module…

Artikel-Nr. 7890002

Version 1.0

Number of days until event

The module cyclically calculates the difference between a target date and the current date. The number of days until the target date is reached is sent out at the outputs. In…

Artikel-Nr. 7890047

Version 1.0

Window (tilted)

The function template displays the status of a window (open or tilted). It enables operating the window via KNX when electric motor drives are also used.

Artikel-Nr. 7890076

Version 2.0

Bar graph

The sample project shows a measured value for the current day and the past 7 days in the form of a bar graph within the MiniVisu.

Artikel-Nr. 7890039

Version 1.0

FanCoil

The function template is used to operate and display the status of fan coil controllers. The number of fan speeds can be selected via the behaviour.

Artikel-Nr. 7890081

Version 2.1

Fan controller

The function template is used to operate and display the status of fan controllers. The number of fan speeds can be selected via the behaviour. The following behaviours are…

Artikel-Nr. 7890082

Version 2.0

Gira KNX alarm control unit

The KNX alarm control unit plug-in is used in connection with the Gira alarm control unit KNX (Order Number 1142 00) to display the current system states of the alarm control unit…

Artikel-Nr. 7890092

Version 1.1

Resources

The Resources plug-in is used to visualise current measured values and display balances or progressions. The following energy types can be visualised with the plug-in. 1…

Artikel-Nr. 7890101

Version 2.1

Audio universal

The function template is used to represent individual displays/operations for up to 4 1-bit communication objects from the audio range. The number of fields (1-4) and the symbols…

Artikel-Nr. 7890108

Version 1.0

Audio sources with volume

The function template is used to change over the source and set the volume of audio sources. The number of sources and the use of the mute function are determined using parameters…

Artikel-Nr. 7890109

Version 1.0

Universal (1Bit)

The function template is used to represent individual displays/operations for up to 4 1‑bit communication objects. The number of fields (1-4) and the symbols to be displayed are…

Artikel-Nr. 7890110

Version 1.0

HomeServer: ScenarioPro

ScenarioPro eröffnet dem Integrator in Sachen Szenen völlig neue Möglichkeiten. Da sich Szenen jederzeit inkl. der zugerhörigen Objekte gebäudeweit anlegen und ändern lassen, muss…

Version 1.0

HomeServer: QC-Camera

Mit QC-Camera können Videostreams von IP-Kameras im Gira QuadClient dargestellt werden. QC-Camera unterstützt alle gängigen Videoformate, Codecs und Auflösungen inklusive des…

Version 1.1

Raumtemperaturregler Heizen

Der Logikbaustein wird zur Einzelraum-Temperaturregelung verwendet. In Abhängigkeit der Betriebsart, des aktuellen Temperatur-Sollwerts und der Raumtemperatur kann für einen…

Artikel-Nr. 7890097

Version 1.0

Raumtemperturregler Kühlen

Der Logikbaustein wird zur Einzelraum-Temperaturregelung verwendet. In Abhängigkeit der Betriebsart, des aktuellen Temperatur-Sollwerts und der Raumtemperatur kann für einen…

Artikel-Nr. 7890098

Version 1.0