Query function in the QuadClient (browser plug-in)
The sample project contains a query function for 15 group addresses which can be switched on/off via the building structure of the QuadClient. The states are visualised within the…
Folgende Dateien sind nicht in der von Ihnen gewählten Sprache verfügbar, aber eventuell in anderen Übersetzungen.
The sample project contains a query function for 15 group addresses which can be switched on/off via the building structure of the QuadClient. The states are visualised within the…
The sample project shows a measured value for the current day and the past 7 days in the form of a bar graph within the MiniVisu.
Sample project for controlling the DCS Communicator via UDP telegrams from the visualisation of the HomeServer.
Sample project for controlling the HSPlugInClient via IP telegrams from the visualisation of the HomeServer.
The sample project for the ETS 4 shows the parameterisation of the KNX presence detector Comfort (Gira Order No. 2106 xx) as a main unit with 2 auxiliary units and a switching…
The sample project for the ETS 4 shows the parameterisation of the KNX presence detector Comfort (Gira Art. No. 2106 xx) as an individual device in the function ceiling observer…
The sample project for the ETS 4 shows the parameterisation of the KNX presence detector Comfort (Gira Order No. 2106 xx) as an individual device in the function "Presence detector…
The sample project for the ETS 4 shows the parameterisation of the KNX presence detector Comfort (Gira Order No. 2106 xx) for an office application with light control and…
The sample project contains a complete template for realising a query function in the QuadClient with the functions of the main menu icons and function templates from Expert…