Garbage notification
The logic module calculates cyclically repeating collection dates and provides information about upcoming collection of a garbage type (e.g. bio-waste, green bin). One module…
Folgende Dateien sind nicht in der von Ihnen gewählten Sprache verfügbar, aber eventuell in anderen Übersetzungen.
The logic module calculates cyclically repeating collection dates and provides information about upcoming collection of a garbage type (e.g. bio-waste, green bin). One module…
Realises automatic watering of the garden depending on a weather station with rain sensor, the cistern fill level and the forecast chance of rain without additional sensors.
The module is for calculation of the dewpoint depending upon relative humidity in % and air temperature.
The module is for calculation of the frost point depending upon relative humidity in % and air temperature.
The logic module keeps the desired brightness in a room constant based on the measured brightness value.
The module determines the date of the current day as well as the upcoming 7 days and outputs the date as a 14-byte text in the form dd.mm.yyyy for each day.
The global library enables retrieval of Gira device portal weather forecast data using the Gira HomeServer or FacilityServer (HS or FS) and to process this data at communication…
Multi-line display and retentive ring memory of values.
The module determines the date of the current day as well as the past 7 days and outputs the date as a 14-byte text in the form dd.mm.yyyy for each day.
The module illustrates the function of a timer with a freely selectable time. By using several modules, complex sequences can be set up with an editable sequence.
The module cyclically calculates the difference between a target date and the current date. The number of days until the target date is reached is sent out at the outputs. In…
The logic module is used in connection with Gira actuators which support current measurement. Using the current values sent via the bus, the module calculates the current power…
The module uses an ongoing meter reading to calculate the current daily value, the daily value of the previous day, the meter reading of the previous day, the average of the value…
The logic module KNX status (forced) operating mode (1-byte, DPT 20.102) evaluates the 1-byte object "KNX status operating mode" or the object "KNX status forced operating mode" of…
The module is used in connection with the Gira room temperature controllers to evaluate the object "Controller status" in the configuration status controller = controller in…
The module is used in connection with the Gira room temperature controllers to evaluate the object "Controller status" in the configuration status controller = controller in…
The module adds the values of the up to 10 inputs and makes the result available at the output.
The module evaluates group feedback according to DPT 27.001.
The module converts positive integers into the corresponding other number system. In this way, decimal values (max. 32-bit) can be converted into the binary system and output as a…
The module is used to determine the number of active inputs (e.g. open windows) of up to 10 inputs.
The module evaluates a 3-byte telegram according to DPT 232.600 (colour RGB). The HomeServer makes the current values for the RGB colours as 1-byte available at the outputs. The…
The module outputs a 3-byte telegram according to DPT 232.600 (colour RGB). Values in the format 0-255 or in percent can be set for each of the three colours.
A 3-byte value is converted to 24 bits and output via 24 outputs.
The module is used to control fan coils in conjunction with fans in the heating and cooling operating modes in the Automatic or Manual mode. The control of the display elements and…
The module is used to control a 3-speed fan. The basic operation of the fan was modelled on the operation of car air conditioners. Manual mode: Following release, the user can…
The module is used to control a 5-speed fan. The basic operation of the fan was modelled on the operation of car air conditioners. Manual mode: Following release, the user can…
The logic module is used to specify a setpoint value depending on a (KNX room temperature controller) operating mode. The module has been realised to enable operation via the…
The module checks whether the value lies inside or outside a range. The range is defined by an upper and lower limit. If the comparison value is on or below the lower limit, a 1 is…
Der Logikbaustein wird zur Einzelraum-Temperaturregelung verwendet. In Abhängigkeit der Betriebsart, des aktuellen Temperatur-Sollwerts und der Raumtemperatur kann für einen…
Der Logikbaustein wird zur Einzelraum-Temperaturregelung verwendet. In Abhängigkeit der Betriebsart, des aktuellen Temperatur-Sollwerts und der Raumtemperatur kann für einen…
This module switches the selected input to the output. The output is then given the value of the selected input. This module could bes used to switch a system between the modes…
The module is used to control redundant operation of two HomeServers (HS) or FacilityServers (FS). Function: In connection with a Gira KNX switching actuator, the active HomeServer…
The module evaluates the switching status of RGB(W) lights where feedback is separate for each colour component through a 1-byte object and no feedback object is available for the…
The logic node is used in conjunction with the KNX gateway from the company Schüco in order to evaluate the latest status or event information from the Schüco system. Hint: The…
Control of Schüco windows and Schüco sliding systems.
Steuerung und Integration kompatibler sonoro Musiksysteme in Gira Smart-Home-Umgebungen. Die Anwendung ermöglicht die zentrale Bedienung wichtiger Audiofunktionen direkt über den…